We offer you two payment options based on performance:
1. Financed model based on energy performance contracting (EPC)
Let the savings in utility costs pay for the project directly. Danfoss offers a model in which a part of the achieved savings pays for the project. This model has a positive cash flow to client throughout the project. Each contract year a reconciliation is made.
2. Client financed payment based on performance
Payment is split in 4 instalments each representing a milestone of the EnSave® project. At the 4th milestone, typically after 2 years, reconciliation* is made.